Product FAQs

Ask a Question

What are the main difference between Evolis 17.5 kV and Evolis 24 kV ?

Even if the brand name is identical and it is 2 vacuum circuit breakers, these two ranges are very different :

 
Was this helpful?
What can we do to improve the information ?