Product FAQs

Ask a Question

Where to configure communications to an ADVC controller in WSOS5?

Issue
User needs to know where in WSOS5 to communications settings are configured

Product Line
ADVC Reclosers

Environment
WSOS5

Resolution
The communications must be configured to communicate to an ADVC controller.

This menu is located: Customize > WSOS communications > Select the communications protocol/method (Typically Direct) and configure the parameters accordingly.

In most cases Direct will be used and the only parameter that must be configured is the Comms Channel. The Comms Channel is the communications port used on the PC, this may be verified using the Device manager built within Windows.

Was this helpful?
What can we do to improve the information ?