Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
What programming languages can be used with the Quantum Safety PLC?
Only Unity Pro XLS V7.0 can be used to program the Quantum Safety PLC. Unity Pro XLS V13.0 does not support the Quantum Safety product line.
For programming your SIL2 project, you are only allowed to use the following 2 programming languages:
- function block diagram (FBD)
- ladder diagram (LD)
Both are languages defined by the IEC 61131-3 for the programming of PLCs.
Did this answer your question?