Product FAQs

Ask a Question

What Modbus parameters are available for port 1 on a Twido for programming?

The Twido only supports one Modbus port parameter for programming.
 

Baud Rate
19,200
Parity
None
Data Bits
8
Stop Bits
1

Note: The Twido line was obsoleted Dec. 2015 and replaced wit the M221 line. For more information on this contact local distributor or technical support.
Was this helpful?
What can we do to improve the information ?