Product FAQs

Ask a Question

How can I update I/O data faster than normal scan time solve in Quantum and high end Compact (PC-E984-258/265/275/285) Controllers?

984 Ladder Logic has a Immediate I/O (IMIO) Instruction which will interrupt the PLC scan and give immediate access to I/O. When the instruction is solved, the IMIO will take information from an input module and place into the State Ram or It can take information from the State Ram and transfer the data to an output module. This happens within the scan compared to a normal solve of read inputs per the segment scheduler and write outputs per the segment scheduler.



Note: The Quantum controllers and the Compact controllers are obsolete have been replaced by the M340 and M580 controller families, for more information on this contact your local distributor or Schneider Electric sales office.
Was this helpful?
What can we do to improve the information ?