Product FAQs

Ask a Question

Why can't I see my descriptors after importing a Taylor 484 program using ProWORX 32?

When importing a Taylor 484 program using ProWORX 32, the descriptors do not get imported. In order to get the descriptors into the new ProWORX 32 Project, you need to export them as a Taylor ASCII file using the Taylor 484 Utility and then import them into ProWORX 32 using the "Import Documentation" function.

Note: Proworx software is obsolete and upgrading the hardware and the software to Unity Pro and either the M340, M580, or Unity Momentum, for more information contact your local distributor or Schneider Electric Sales office.


Was this helpful?
What can we do to improve the information ?