Product FAQs

Ask a Question

Does Unity Pro provide system bits to monitor the batteries in the high end Quantum PACs?

%s67 identified as PCMCIABAT0 in Unity Pro monitors the state of the battery in the PCMCIA that resides in the PC Card A slot. (TSX BATM01).
%s75 identified as PCMCIABAT1 in Unity Pro monitors the state of the battery in the PCMCIA that resides in the PC Card B slot. (TSX BATM01).
%s68 identified as PLCBAT in Unity Pro monitors the state of CPU battery that is located behind the slide up LCD display cover.
If these system bits are set to 0, the battery is present and operational. The bits will be set to 1 if there is no battery or the battery is not sufficiently charged.

The smaller battery in the PCMCIA cards (TSX BAT M03) has no diagnostic bit available.

Was this helpful?
What can we do to improve the information ?