Product FAQs

Ask a Question

How can I make a project 'read only' in Concept?

To give a user 'read only' access to a project do the following:
- Open the Concept Security editor.
- Go to the Maintenance tab and <Add> a new user. Give the user a name and assign rights. Hit <OK>.
- Go to the Options tab and check the Password required box for 'Concept program setup'.
<Exit> the Security Editor.
When the user opens Concept for the first time, he logs in without a password and Concept will prompt him to provide a password.
From this point on, all projects that this user opens will be 'read only'.

Was this helpful?
What can we do to improve the information ?