Product FAQs

Ask a Question

What causes 'runtime error 13' in ProWORX 32?

The Runtime Error 13 resides with the Microsoft control comct332.ocx.
To fix this problem:

1) Open a command prompt window.
2) Change the path to the \Windows\System32 folder.
3) Type the command to unregister the ocx file.

regsvr32 -u comct332.ocx

4) Locate and rename comct332.ocx to comct332ocx.old
5) Copy the latest version of this .ocx into the \windows\system32 folder. (see attachment)
6) Open a command prompt window.
7) Change the path to the \windows\system32 folder.
8) Type the command to unregister the OCX file.


regsvr32 comct332.ocx

COMCT332.OCX


Legacy KB System (APS) Data: RESL169778 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?