Product FAQs

Ask a Question

What is the difference between an Analyze and a Build in Unity Pro?

Analyze checks that syntax and semantics are correct but doesn't Build the application.
Build creates the executable code for the PLC application. Build or Rebuild automatically does an Analyze.
'Rebuild all' should only be used on a first build, a modification of project settings or hardware configuration.


Legacy KB System (APS) Data: RESL170812 V1.0, Originally authored by on , Last Edited by on
Related ranges: Unity Pro
Was this helpful?
What can we do to improve the information ?