Product FAQs

Ask a Question

What are the part numbers for the 800 I/O to Quantum Conversion Connector Swing Arms?

The Conversion Connector Swing Arms are available in Aluminum and Steel for 19" and 27" installations. The part numbers for each are listed below:

text
Part Number
text
Description
text
990QFCSWM19A
text
19" Aluminum Swing Arm
text
990QFCSWM19S
text
19" Powder Coat Steel Swing Arm
text
990QFCSWM27A
text
27" Aluminum Swing Arm
text
990QFCSWM27S
text
27" Powder Coat Steel Swing Arm


 
Was this helpful?
What can we do to improve the information ?