Product FAQs

Ask a Question

What causes error "line xxx: error storing value in attribute" when opening a Concept RDE template?

This can occur if the option "Allow leading digits" is enabled or if the RDE template contains a variable such as, "012Enn" where nn=01-99.
The RDE sees the variable as a float in exponent representation.
(Note: Corrected in Version 2.6 SR1D).


Legacy KB System (APS) Data: RESL171862 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?