Product FAQs

Ask a Question

What does error 151 generated by the Xxmit block mean?


Error 151 indicates the variables associated with MsgOut / MsgIn parameters are not long enough. When the Xxmit block is being used as a Modbus messaging function the MsgIn and MsgOut parameters must be configured as located variable of type Word Array 9.


Legacy KB System (APS) Data: RESL172843 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?