Product FAQs

Ask a Question

Why is the 'archive' option greyed out in Concept?

The Archive function is only available when there are no projects open.
Note: This is also true of the optimize function.


Legacy KB System (APS) Data: RESL173663 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?