Product FAQs

Ask a Question

Which ModbusTCP services do the PowerLogic EGX Modbus to Ethernet Gateways support?

The PowerLogic EGX200 and EGX400 Gateways support the ModbusTCP Server, BootP Client, Embedded Web diagnostics, FTP, TFTP, SNMP v1, and Telnet Server for additional diagnostics. Though they support TFTP, the EGX Gateways do not support FDR.


Legacy KB System (APS) Data: RESL173854 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?