Product FAQs

Ask a Question

What changes/updates are included in Proworx Nxt 2.2 SR6A?

Special 6a Features
----------------------------------------------
- New support for Quantum CPS114-20, CPS124-20 modules.
- New support for Quantum NOE771-01, NOE771-11 modules.
- New support for bootp of Momentum ENT module.
- New support for Compact DEP-256, DAP-258, ADU-256 modules.
- New support for Quantum NOA622 module.
- New support for Momentum ANR120-91 module.

- Fixed search descriptor causing Illegal Function Call when connected TCP/IP.
- Fixed selection of M7251 or M7350 modules from drop down list.
- Fixed timeout on Modbus RTU connected to Momentum 760-00 when searching.
- Fixed monitor LAN only seeing 11 nodes.
- Fixed short comment copy of 4xxxx bit descriptors.
- Fixed maximum allowed digits in modem phone number (now supports 50)


Legacy KB System (APS) Data: RESL174018 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?