Product FAQs

Ask a Question

What changes/updates are included in Nxt 2.2 SP8?

Special 8 Features
----------------------------------------------
- Fixed DDO364-00 User Defined/Last Value settings.
- Fixed CPS 114-20, CPS 124-20 editing and power ratings.
- Fixed NOE771-11 card causing an error "File not Found" in the TCOP editor
- Fixed partial write of state ram clearing logic unintentionally.
- Removed "Restore PLC Run State Before Power Down" option on the Transfer to Flash dialog for Momentum controllers.


Legacy KB System (APS) Data: RESL174020 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?