Product FAQs

Ask a Question

Which Advantys PDM module is used with the Relay output modules?

When using either the STBDRC3210 or the STBDRA3290 relay output module, the required PDM module would have to be a DC PDM (STBPDT3100 or STBPDT3105). An AC PDM will not be compatible with the relay output modules.



R-120517
 


Legacy KB System (APS) Data: RESL176649 V1.0, Originally authored by on , Last Edited by on
Related ranges: Advantys STB
Was this helpful?
What can we do to improve the information ?