Product FAQs

Ask a Question

What does "BUSY" mean when I do a "Netscan" with ProWORX NxT?

Title
What does "BUSY" mean when I do a "Netscan" with ProWORX NxT?

Issue
"BUSY" meaning when I do a "Netscan" with ProWORX NxT

Product Line
ProWORX NXT

Environment
ProWORX NXT

Cause
When doing a "Netscan" with ProWOX NxT, "BUSY" means that the Modicon PLC is already "Logged On" for Programming privilege by another computer. Only 1 Programming Device can be "Logged On" at any one time.

Resolution
 To correct the problem, you must find out which computer is "Logged On" and "Log Off".

Was this helpful?
What can we do to improve the information ?