Product FAQs

Ask a Question

Are the RA1X and RA3X loadables supported?

No. These loadables were not developed by Schneider. They are similiar in function to the older 1X , 3X blocks used in 984LL.
As Schneider did not officially author the RA1X/RA3X blocks we cannot be responsible for their functionality or compatability in our product lines.
 


Legacy KB System (APS) Data: RESL180348 V1.0, Originally authored by DaSo on 10/12/2006, Last Edited by DaSo on 10/12/2006
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?