Product FAQs

Ask a Question

What is included with the USB to Modbus Plus converter TSXCUSBMBP?

The TSXCUSBMBP converter includes a CD which has the driver, a user's guide, and a diagnostic tool especially designed for Modbus Plus networks. 

Driver Compatibility (Version 9.0):
Windows 10 / 8 / 7 SP1
Windows Server 2016 / 2012 / 2008 R2 SP1

Was this helpful?
What can we do to improve the information ?