Product FAQs

Ask a Question

Are there any restrictions on where modules can be placed in a Modicon M340 rack?

Yes, The left most slot of the rack is reserved for the power supply. The next slot is considered slot 0 and it is reserved for the CPU.
The remaining slots numbered 1 - 11 (BMXXBP1200) can be used for I/O modules. Any module in any slot.


Legacy KB System (APS) Data: RESL187213 V1.0, Originally authored by DaSo on 07/23/2007, Last Edited by DaSo on 07/23/2007
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?