Product FAQs

Ask a Question

What is the definition of Global Data in Concept?

The Global Data defines the memory space for unlocated variables.
The total Global Data used is available under the Memory Statistics.
Schneider Electric recommends keeping the Configured Global data 20 % higher than the used Global data to allow download changes without any problems.

Note: Any changes to the Global Data will require the user to do a complete download to the PLC in order to re-connect EQUAL.

Was this helpful?
What can we do to improve the information ?