Product FAQs

Ask a Question

Does the TwidoSuite Simulator support the PID function?

No, simulation mode does not work with PID or any of the following functions FC, VFC, PLS/PWM and EXCH.

Note: The Twido line was obsoleted 12/31/15 and has been replaced whth the M221 product line it is the direct replacement for the Twido and the program can be imported into it using the SoMachine Basic software that is a free download.
Was this helpful?
What can we do to improve the information ?