Product FAQs

Ask a Question

Can the new Twido T2M I/O modules only be configured in TwidoSuite 2.20 and above?

No.In TwidoSoft, all versions will need to be configured to the old module from the pick list and the same goes for all versions of TwidoSuite less than 2.20.

Note: Twido was obsoleted in Dec. 2015 and was replaced with the M221 and SoMachine Basic. The M221 will support the TM2 I/O modules in SoMachine Basic.
Was this helpful?
What can we do to improve the information ?