Product FAQs

Ask a Question

Are there replacements for Modbus Plus TIO modules?

Title
Are there replacements for Modbus Plus TIO modules?

Issue
Replacements for Modbus Plus TIO modules

Product Line
Modicon Momentum

Environment
Modbus Plus

Cause
Product Obsolescence

Resolution
The following product substitution table lists the Modbus Plus TIO modules along with the replacement Momentum I/O module base and Modbus Plus communications adapter.

text
Modbus Plus TIO Module
text
Momentum I/O Module Base
text
Modbus Plus Comm. Adapter
text
170BDI34200
text
170ADI34000
text
170NEF11021
text
170BDO34200
text
170ADO34000
text
170NEF11021
text
170BDM34200
text
170ADM35010
text
170NEF11021
text
170BDI54250
text
170ADI54050
text
170NEF11021
text
170BDO54250
text
170ADO54050
text
170NEF11021
Was this helpful?
What can we do to improve the information ?