Product FAQs

Ask a Question

Is there a way to check the 'Save' attribute on all variables at the same time?

Yes. Double click on Elementary Variables in the Project Browser. Right click on the Variables and choose 'Select All'. Right click again and choose 'Data Properties'. Go to the Data Properties box on the left side of the screen and click on the 'Save' attribute. This should check the 'Save' attribute in all the variables in the Variable Editor.

Was this helpful?
What can we do to improve the information ?