Product FAQs

Ask a Question

What is the part number of the cable that is used to connect a Magelis HMISTO to the Twido Mini-din port?

The part number of the cable is XBTZ9780.


Note The Twido product line is obsolete and has been replaced with the M221 product line. The M221 does not use the mini din type connector but either a RJ45 or a terminal connection. 
Was this helpful?
What can we do to improve the information ?