Product FAQs

Ask a Question

What is the maximum number of input and output words allowed on the local Quantum drop when programming with Unity?

There are no limits to the number of input words and/or output words on the local drop. The only limitation will be the number of available module slots in the backplane.


Legacy KB System (APS) Data: RESL210947 V1.0, Originally authored by DaSo on 03/13/2013, Last Edited by DaSo on 03/13/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?