Product FAQs

Ask a Question

What is the maximum bus length for the Quantum 140EIA92100 AS-i module?

 

        • Max length of the bus": 100m.
          Possibility to extend the bus through repeaters (+supplies): 2 repeaters max between the master and a slave (300m).
          Scan Time: 5ms with 31 stations / 10ms with 62 stations with extended profile.
           

Was this helpful?
What can we do to improve the information ?