Product FAQs

Ask a Question

Are there any isolated analog input modules available in the Advantys STB I/O offer ?

Yes, there are two analog input modules which are isolated. The STBAVI0300, analog voltage input module and the STBACI0320, analog current input module.


R-120517


Legacy KB System (APS) Data: RESL211368 V1.0, Originally authored by DaSo on 05/04/2013, Last Edited by DaSo on 05/04/2013
Related ranges: Modicon STB
Was this helpful?
What can we do to improve the information ?