Product FAQs

Ask a Question

What does the +, -, and not equal mean when on-line with TwidoSuite?

This shows the hardware and if it is configured, not configured or hardware not detected.



Note: The Twido line has been obsolete since 2015 and replaced with the M221 product family, you can import your Twido project into SoMachine Basic and use the same I/O as long as it is the TM2 modules. For more questions contact your local distributor os Schneider sales office.
Was this helpful?
What can we do to improve the information ?