Product FAQs

Ask a Question

Are there any parts of a Twido PLC that are field replaceable?

Issue:
Any of the Twido parts are field replaceable.

Product Line:
Twido

Cause:
Bad input or output and field terminals.

Resolution:

There are no parts on the Twido PLC that are replaceable not even the field connectors they are soldered into the Twido controller. The entire Twido controller must be replaced. The Twido line is obsolete and it is recommended that the Twido should be replaced with the M221 family.


Was this helpful?
What can we do to improve the information ?