Product FAQs

Ask a Question

Why don't my %MW initial values get written to my M340 when I perform a full project transfer to PLC?

This is probably due to the fact that the "Initialize %MWi on cold start" selection is unchecked in the PLCs configuration tab. This setting must be checked in order for the initial values to be sent to the PLC during a full transfer of the project.

Was this helpful?
What can we do to improve the information ?