Product FAQs

Ask a Question

What is the part number of the cable that is needed to communicate from a XBTN400 to a Twido mini din port?

Cable for the Magelis XBTN400 to a Twido mini din is the XBTZ9780.


Note: The Twido is obsolete and it is recommended to upgrade to the M221 and that will have a RJ45 connection and can use the XBTZ9980.
Was this helpful?
What can we do to improve the information ?