Product FAQs

Ask a Question

Is it possible to prevent the Unity HSBY system from generating an offset or +1 Modbus I/P address ?

No. You cannot inhibit the Unity HSBY system from generating the offset or +1 address.


Legacy KB System (APS) Data: RESL212996 V1.0, Originally authored by DaSo on 11/13/2013, Last Edited by DaSo on 11/13/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?