Product FAQs

Ask a Question

What is the minimum clearance for mounting Twido Controllers in a cabinet?

Minimum Clearances for a Compact Controller and Expansion I/O Modules. In order to maintain a natural circulation of air around the Compact controller and expansion I/O modules in a control panel, observe the minimum clearances shown in the figures below.

Minimum Clearances for a Modular Controller and Expansion I/O Modules. In order to maintain a natural circulation of air around the Modular controller and expansion I/O modules in a control panel, observe the minimum clearances shown in the figures below.

 


Note: Twido was made obsolete 12/1/2015 and has been replaced with the M221. The Twido program can be imported into the M221 SoMachine Basic software and the dimensions are the same for the M221 as the Twido. For further information on this contact your local distributor or Schneider sales office.
Was this helpful?
What can we do to improve the information ?