Product FAQs

Ask a Question

Can the EM35xx meter act as a gateway and read registers from a downstream Modbus device?

Issue
User would like to know if the EM3560 meter can be used as a gateway device to read downstream Modbus slaves

Product Line
Energy Meter EM35xx series

Environment
Communications

Resolution
The EM35xx series of meters cannot act as a gateway. These devices operate in slave mode only. Therefore, the meter cannot read downstream devices or convert protocols.

Was this helpful?
What can we do to improve the information ?