Product FAQs

Ask a Question

Is there a limit to the number of I/O Events that can be used with a Quantum processor in Unity?

There is a limit.  It is possible to have up to 128 I/O Events,  numbered 0-127.

Was this helpful?
What can we do to improve the information ?