Product FAQs

Ask a Question

Is there a PCMCIA card converter that will allow me to use my Modbus Plus PCMCIA Type III card in a laptop computer that only has Type II slots?

Laptops now have only one Type II PCMCIA slot and our 416NHM21234 will only fit in Type III slots.
An extender card will allow the Modbus Plus PCMCIA card to work in current laptops.

The extender card has all signals passing straight through ( one to one pinout ).

This information can also be found on the retailers Web site at: http://www.twinhunter.com

The product part number for this product is: 3300-EXT

 
 
 
 
3300-EXT PCMCIA 2 Layer Extender

Board Size: 2.125"x6.35"
    • Two layer design.
    • All signals are passed straight through.
    • The 3300-EXT extends the Unit Under Test out of the system for easy access.
    • The 3300-EXT extends the life of your system by absorbing the wear and tear of multiple insertion environments.


 
text text text text

Was this helpful?
What can we do to improve the information ?