Product FAQs

Ask a Question

Does the Unity Loader require an authorization?

The Unity Loader is a stand-alone software tool dedicated to the M340, Premium and Quantum hardware platforms. A Unity Pro license is not required to use the loader.

  • The Unity Loader software provides the following transfer features:
    • - transfer of a Unity Pro application from a PC to a Modicon M340, Premium or Quantum PLC.
      - transfer of a Unity Pro application from a Modicon M340, Premium or Quantum PLC to a PC.
      - transfer of firmware (FW) from a PC to a Modicon M340 PLC or to a module with firmware of the Modicon M340 platform.

      Note: The Unity Loader software requires one of the following operating systems:
      Microsoft Windows XP Professional

      Microsoft Windows Vista Business

      Microsoft Windows 7 Professional

      M340_system_bits_words.zipM340_system_bits_words.zip

Was this helpful?
What can we do to improve the information ?