Product FAQs

Ask a Question

When configuring the 140DRC83000, which bits are used of the User Defined Timeout State field?

For the User Defined Timeout State of the 140DRC83000, only the bits of the low byte or right most byte are used.
For example a value of 00FF Hex, will set all outputs high on a timeout condition.
Was this helpful?
What can we do to improve the information ?