Product FAQs

Ask a Question

What Cablefast block can be used with the 140DRA84000 relay card?

The only block that can be used is the 140CFA04000 block and it is a straight through block. The only limitation on it is that you can not exceed .5 amps per point.
Was this helpful?
What can we do to improve the information ?