Product FAQs

Ask a Question

Where can I find the SoMove modbus driver for Windows XP and Windows 7?

Issue:
Where can I find the SoMove modbus driver for Windows 10 and Windows 7?

Product Line:
SoMove

Environment:
All

Cause:
Modbus Drivers

Resolution:
SoMove should automatically install the ModBus drivers, so an additional download should not be needed.
However the files can be downloaded from this website link:  http://bricks-portal.schneider-electric.com/Domain/SW%20Device%20Platform/Domain/SW%20Device%20Platform/PC%20Communication%20Drivers/Modbus%20SL%20Drivers/Modbus%20SL%20Drivers/EngineeringView/index_html
Registration on this site is required.  It is not clear if this site is available to those outside Schneider Electric and for that reason the FAQ has been marked as Internal.

NOTE: 
Windows XP is no longer supported by SoMove
Was this helpful?
What can we do to improve the information ?