Product FAQs

Ask a Question

Are the digital inputs for the VAMP 321 polarity sensitive?

Issue
When wiring the input does it matter which one the negative or positive is wired into?

Product Line
VAMP 321

Resolution
No the digital inputs are not polarity sensitive.

 
Was this helpful?
What can we do to improve the information ?