Product FAQs

Ask a Question

Which Modem is recommended to be used with SoMachine V4.3 and the M238 controller?

The only Modem we tested with the M238 is the SR2MOD03.
 
With this modem you can do the following:
- Using GSM modem, it is possible to send/receive SMS
- Using SMS or RTC modem,
- it is possible to establish communication between two PLCs in order to exchange data via Modbus.
 
 
Was this helpful?
What can we do to improve the information ?