Product FAQs

Ask a Question

Can a repeater be used in a Twido remote link network?

No. The remote link uses a proprietary protocol and no third party devices like a repeater will work on the network.


Note: The Twido product line was obsoleted in Dec. 2016 and has been replaces with the M221, it is a direct replcement for the Twido and the same I/O can be use and program imported into the SoMachine Basic software that is a free download.
Was this helpful?
What can we do to improve the information ?