Product FAQs

Ask a Question

Is there a known issue of import failures of Legacy Momentum Applications into Unity Pro?

Title
Is there a known issue of import failures of Legacy Momentum Applications into Unity Pro 8.0?

Issue
When a Legacy Momentum project is being converted from a Legacy software to Unity Pro 8.0 the error below appears.


Enviroment
Unity Pro

Product Line
Momentum

Cause
There is no I/O Configured in the Legacy project.

Resolution
To solve the issue, one or more Momentum I/O bases must be added to the Legacy configuration.
Was this helpful?
What can we do to improve the information ?