Product FAQs

Ask a Question

What is the compatibility between Switch2Vijeo tool version and Vijeo Designer versions

The compatibility between Switch2Vijeo tool version and Vijeo Designer versions for application program conversion is as tabulated below :
 
 
XBTL1000 Application Program Switch2Vijeo Version
VJD 4.5 S2VJD 1.0
VJD 4.6 S2VJD 2.0
VJD 4.6 Patch D S2VJD 2.1
VJD 4.7 S2VJD 2.2
VJD 5.0 S2VJD 3.0
VJD 5.0 SP1 S2VJD 3.1
Was this helpful?
What can we do to improve the information ?