Product FAQs

Ask a Question

Using SoMachine controller, can the visualization be viewed using the web server interface?


Title:
 

Using SoMachine controller, can the visualization be viewed over the web server interface?
 

Issue:

Customer wants to view the visualization on a SoMachine controller and wants to view the visualization using the web server interface.

Product Line:

SoMachine Controller
 

Environment:

SoMachine ver 3.1, Webserver
 

Cause:

Not applicable
 

Resolution:

No, it is not possible to view the visualization using the web server interface.
Was this helpful?
What can we do to improve the information ?